K60 LQFP Package: When?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 LQFP Package: When?

ソリューションへジャンプ
5,426件の閲覧回数
Alberto_g
Contributor III

A non-BGA package would be easier for us. It was announced, when will it be available? 144 pins.

 

Regards.

0 件の賞賛
返信
1 解決策
4,772件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Alberto,

 

There are some chips available in 144 pin LQFP package now:

 

* PK60N256VMD100

* PK60N512VLQ100

* PK60X256VLQ100

 

Now, these are only samples. Production is expected to begin by Q3, 2011.  This is not a deffinite date, but an approximate.

 

Are you working on a project for a company ?

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,773件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Alberto,

 

There are some chips available in 144 pin LQFP package now:

 

* PK60N256VMD100

* PK60N512VLQ100

* PK60X256VLQ100

 

Now, these are only samples. Production is expected to begin by Q3, 2011.  This is not a deffinite date, but an approximate.

 

Are you working on a project for a company ?

0 件の賞賛
返信
4,772件の閲覧回数
Alberto_g
Contributor III

Yes, I see that now the "Buy/Parametrics" page offers the TQFP package.

We are evaluating this component for some industrial control boards. Mainly it should be a Eth to CANBus gateway.

 

Many thanks.

0 件の賞賛
返信
4,772件の閲覧回数
pende
Contributor III

Hello,

 

when do you expect to begin the production of the 1 MB Flash and 196/256 Packages of K60?

 

Regards, Philip

 

0 件の賞賛
返信
4,772件の閲覧回数
pende
Contributor III

pende wrote:

Hello,

 

when do you expect to begin the production of the 1 MB Flash and 196/256 Packages of K60?

 

Regards, Philip

 


pushing to renew the thread,

0 件の賞賛
返信
4,772件の閲覧回数
iggi
NXP Employee
NXP Employee

The expectation is that, it will start in Q4 2011

0 件の賞賛
返信