K60 FlexCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 FlexCAN

4,241件の閲覧回数
vasyapupkin
Contributor I

I can not turn on the receiver FIFO (CAN_LDD component)

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

3,756件の閲覧回数
vasyapupkin
Contributor I

Hello Vojtech Filip.

I use CW10.4 and TowerKit K60F120M.

PE when choosing ReceiverFIFO says: "ERROR The component doesn't support this setting!"

What are the component settings prohibit enable FIFO?

Or component does not support FIFO?

0 件の賞賛
返信

3,756件の閲覧回数
vasyapupkin
Contributor I

In reference to the component written:

     Receiver FIFO - Enable/Disable receiver FIFO feature.

        The following items are available only if the group is enabled (the value is "Enabled")

Where to allow this?

0 件の賞賛
返信

3,756件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

this feature is currently supported only for MSCAN device. As workaround you could use "Message buffers" or freeze the code of this component and implement it manually. I have also passed request to support FIFO feature to developers.

We are sorry for inconvenience.

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信

3,756件の閲覧回数
ninestone
Contributor II

I've run into the same issue on a Kinetis device.  I hope this will be supported in the near future.

0 件の賞賛
返信

3,756件の閲覧回数
vasyapupkin
Contributor I

Thank you for your help. I will implement manually.

0 件の賞賛
返信

3,756件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hello,

could you please provide more details? What version of CW do you use? What MCU, etc.?

The best way would be to post here the ProcessorExpert.pe file from your project and provide info about CW verison that you use.

Best regards

Vojtech Filip

Processor Expert Support Team

0 件の賞賛
返信