Hi,
I use K60 FlexBus to read/write CPLD in 16-bit data and 10-bit address mode.
HW setting:
//FlexBus
//Address
PORTB_PCR20 = PORT_PCR_MUX(5); // fb_ad[31] - FB_XA15
PORTB_PCR21 = PORT_PCR_MUX(5); // fb_ad[30] - FB_XA14
PORTB_PCR22 = PORT_PCR_MUX(5); // fb_ad[29] - FB_XA13
PORTB_PCR23 = PORT_PCR_MUX(5); // fb_ad[28] - FB_XA12
PORTC_PCR12 = PORT_PCR_MUX(5); // fb_ad[27] - FB_XA11
PORTC_PCR13 = PORT_PCR_MUX(5); // fb_ad[26] - FB_XA10
PORTC_PCR14 = PORT_PCR_MUX(5); // fb_ad[25] - FB_XA9
PORTC_PCR15 = PORT_PCR_MUX(5); // fb_ad[24] - FB_XA8
PORTB_PCR6 = PORT_PCR_MUX(5); // fb_ad[23] - FB_XA7
PORTB_PCR7 = PORT_PCR_MUX(5); // fb_ad[22] - FB_XA6
PORTB_PCR8 = PORT_PCR_MUX(5); // fb_ad[21] - FB_XA5
PORTB_PCR9 = PORT_PCR_MUX(5); // fb_ad[20] - FB_XA4
PORTB_PCR10 = PORT_PCR_MUX(5); // fb_ad[19] - FB_XA3
PORTB_PCR11 = PORT_PCR_MUX(5); // fb_ad[18] - FB_XA2
PORTB_PCR16 = PORT_PCR_MUX(5); // fb_ad[17] - FB_XA1
PORTB_PCR17 = PORT_PCR_MUX(5); // fb_ad[16] - FB_XA0
//Data
PORTB_PCR18 = PORT_PCR_MUX(5); // fb_ad[15] - FB_XD15
PORTC_PCR0 = PORT_PCR_MUX(5); // fb_ad[14] - FB_XD14
PORTC_PCR1 = PORT_PCR_MUX(5); // fb_ad[13] - FB_XD13
PORTC_PCR2 = PORT_PCR_MUX(5); // fb_ad[12] - FB_XD12
PORTC_PCR4 = PORT_PCR_MUX(5); // fb_ad[11] - FB_XD11
PORTC_PCR5 = PORT_PCR_MUX(5); // fb_ad[10] - FB_XD10
PORTC_PCR6 = PORT_PCR_MUX(5); // fb_ad[9] - FB_XD9
PORTC_PCR7 = PORT_PCR_MUX(5); // fb_ad[8] - FB_XD8
PORTC_PCR8 = PORT_PCR_MUX(5); // fb_ad[7] - FB_XD7
PORTC_PCR9 = PORT_PCR_MUX(5); // fb_ad[6] - FB_XD6
PORTC_PCR10 = PORT_PCR_MUX(5); // fb_ad[5] - FB_XD5
PORTD_PCR2 = PORT_PCR_MUX(5); // fb_ad[4] - FB_XD4
PORTD_PCR3 = PORT_PCR_MUX(5); // fb_ad[3] - FB_XD3
PORTD_PCR4 = PORT_PCR_MUX(5); // fb_ad[2] - FB_XD2
PORTD_PCR5 = PORT_PCR_MUX(5); // fb_ad[1] - FB_XD1
PORTD_PCR6 = PORT_PCR_MUX(5); // fb_ad[0] - FB_XD0
//Control signals
PORTB_PCR19 = PORT_PCR_MUX(5); // fb_oe_b
PORTC_PCR11 = PORT_PCR_MUX(5); // fb_rw_b
PORTD_PCR1 = PORT_PCR_MUX(5); // fb_cs0_b to CPLD
PORTC_PCR18 = PORT_PCR_MUX(5); // fb_cs2/b
PORTD_PCR0 = PORT_PCR_MUX(5); // fb_ale
PORTC_PCR3 = PORT_PCR_MUX(5); // CLKOUT
FlexBus initial code:
#define CPLD_ADDR (*(vuint16*)(0xA0000000))
FB_CSAR0 = (uint32)&CPLD_ADDR;
FB_CSMR0 = FB_CSMR_BAM(7) //Set base address mask for address space
| FB_CSMR_V_MASK ; //Enable CS signa
FB_CSCR0 = FB_CSCR_PS(2) // 16-bit port
| FB_CSCR_AA_MASK // auto-acknowledge
| FB_CSCR_ASET(0x1) // assert chip select on second clock edge after address is asserted
| FB_CSCR_WS(0x1) // 1 wait state - may need a wait state depending on the bus speed
| FB_CSCR_BLS_MASK;
Write to CPLD:
uint16 CPLDdata = 0x1234;
*(vuint16*)(&CPLD_ADDR) = CPLDdata;
Q1:
If I want to write the next 16-bit data to the next address, the CPLD_ADDR will plus 2 or 1?
For example: 1st address is 0xA0000000, 2nd address will be 0xA0020000 or 0xA0010000?
If plus 2, this means one addree = 8-bit data?
Q2:
In HW connection,(16-bit data mode)
Which connection is right?
1. FB_XA[0-9] <-> CPLD's address[0-9]
2. FB_XA[1-10]<-> CPLD's address[0-9]
Thank you.
Abby