K60 FlexBus 16-bit data, 10-bit address to CPLD

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60 FlexBus 16-bit data, 10-bit address to CPLD

跳至解决方案
2,193 次查看
abby
Contributor I

Hi,

I use K60 FlexBus to read/write CPLD in 16-bit data and 10-bit address mode.

HW setting:

//FlexBus

//Address

PORTB_PCR20 = PORT_PCR_MUX(5);           //  fb_ad[31] - FB_XA15

PORTB_PCR21 = PORT_PCR_MUX(5);           //  fb_ad[30] - FB_XA14

PORTB_PCR22 = PORT_PCR_MUX(5);           //  fb_ad[29] - FB_XA13

PORTB_PCR23 = PORT_PCR_MUX(5);           //  fb_ad[28] - FB_XA12

PORTC_PCR12 = PORT_PCR_MUX(5);           //  fb_ad[27] - FB_XA11

PORTC_PCR13 = PORT_PCR_MUX(5);           //  fb_ad[26] - FB_XA10

PORTC_PCR14 = PORT_PCR_MUX(5);           //  fb_ad[25] - FB_XA9

PORTC_PCR15 = PORT_PCR_MUX(5);           //  fb_ad[24] - FB_XA8

PORTB_PCR6  = PORT_PCR_MUX(5);           //  fb_ad[23] - FB_XA7

PORTB_PCR7  = PORT_PCR_MUX(5);           //  fb_ad[22] - FB_XA6

PORTB_PCR8  = PORT_PCR_MUX(5);           //  fb_ad[21] - FB_XA5

PORTB_PCR9  = PORT_PCR_MUX(5);           //  fb_ad[20] - FB_XA4

PORTB_PCR10 = PORT_PCR_MUX(5);          //  fb_ad[19] - FB_XA3

PORTB_PCR11 = PORT_PCR_MUX(5);           //  fb_ad[18] - FB_XA2

PORTB_PCR16 = PORT_PCR_MUX(5);           //  fb_ad[17] - FB_XA1

PORTB_PCR17 = PORT_PCR_MUX(5);           //  fb_ad[16] - FB_XA0

//Data

PORTB_PCR18 = PORT_PCR_MUX(5);           //  fb_ad[15] - FB_XD15

PORTC_PCR0  = PORT_PCR_MUX(5);           //  fb_ad[14] - FB_XD14

PORTC_PCR1  = PORT_PCR_MUX(5);           //  fb_ad[13] - FB_XD13

PORTC_PCR2  = PORT_PCR_MUX(5);           //  fb_ad[12] - FB_XD12

PORTC_PCR4  = PORT_PCR_MUX(5);           //  fb_ad[11] - FB_XD11

PORTC_PCR5  = PORT_PCR_MUX(5);           //  fb_ad[10] - FB_XD10

PORTC_PCR6  = PORT_PCR_MUX(5);           //  fb_ad[9]  - FB_XD9

PORTC_PCR7  = PORT_PCR_MUX(5);           //  fb_ad[8]  - FB_XD8

PORTC_PCR8  = PORT_PCR_MUX(5);           //  fb_ad[7]  - FB_XD7

PORTC_PCR9  = PORT_PCR_MUX(5);           //  fb_ad[6]  - FB_XD6

PORTC_PCR10 = PORT_PCR_MUX(5);           //  fb_ad[5]  - FB_XD5

PORTD_PCR2  = PORT_PCR_MUX(5);           //  fb_ad[4]  - FB_XD4

PORTD_PCR3  = PORT_PCR_MUX(5);           //  fb_ad[3]  - FB_XD3

PORTD_PCR4  = PORT_PCR_MUX(5);           //  fb_ad[2]  - FB_XD2

PORTD_PCR5  = PORT_PCR_MUX(5);           //  fb_ad[1]  - FB_XD1

PORTD_PCR6  = PORT_PCR_MUX(5);           //  fb_ad[0]  - FB_XD0

//Control signals

    PORTB_PCR19 = PORT_PCR_MUX(5);           // fb_oe_b

    PORTC_PCR11 = PORT_PCR_MUX(5);           // fb_rw_b 

    PORTD_PCR1  = PORT_PCR_MUX(5);           // fb_cs0_b  to CPLD

    PORTC_PCR18 = PORT_PCR_MUX(5);    // fb_cs2/b

    PORTD_PCR0  = PORT_PCR_MUX(5);           // fb_ale

    PORTC_PCR3  = PORT_PCR_MUX(5);    // CLKOUT

FlexBus initial code:

#define CPLD_ADDR   (*(vuint16*)(0xA0000000))

FB_CSAR0 = (uint32)&CPLD_ADDR;

FB_CSMR0  =   FB_CSMR_BAM(7)  //Set base address mask for address space

                         | FB_CSMR_V_MASK ;   //Enable CS signa

                     

FB_CSCR0  =   FB_CSCR_PS(2)      // 16-bit port

             | FB_CSCR_AA_MASK    // auto-acknowledge

             | FB_CSCR_ASET(0x1)  // assert chip select on second clock edge after address is asserted

             | FB_CSCR_WS(0x1)    // 1 wait state - may need a wait state depending on the bus speed

             | FB_CSCR_BLS_MASK;

Write to CPLD:

uint16 CPLDdata = 0x1234;

*(vuint16*)(&CPLD_ADDR) = CPLDdata; 

Q1:

If I want to write the next 16-bit data to the next address, the CPLD_ADDR will plus 2 or 1?
For example: 1st address is 0xA0000000, 2nd address will be 0xA0020000 or 0xA0010000?

If plus 2, this means  one addree = 8-bit data?

Q2:

In HW connection,(16-bit data mode)

Which connection is right?

1. FB_XA[0-9] <-> CPLD's address[0-9]

2. FB_XA[1-10]<-> CPLD's address[0-9]

Thank you.

Abby

0 项奖励
回复
1 解答
1,913 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Abby,

I find you are using FB_AD[31:16] connects with CPLD address lines, which should use FB_A16 & FB_AD[15:1] connects with CPLD address lines(DATA port size is 16-bit).

K60 Flexbus provides extended address line, such as FB_A16, FB_A17 and etc.

So, customer can use FB_AD[31:16] connects with CPLD data lines.

1> CPLD_ADDR will plus 2 (16-bit data port size).

1st address is 0xA0000000, 2nd address will be 0xA0000002.

2> Please refer my above comments. 


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,914 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi Abby,

I find you are using FB_AD[31:16] connects with CPLD address lines, which should use FB_A16 & FB_AD[15:1] connects with CPLD address lines(DATA port size is 16-bit).

K60 Flexbus provides extended address line, such as FB_A16, FB_A17 and etc.

So, customer can use FB_AD[31:16] connects with CPLD data lines.

1> CPLD_ADDR will plus 2 (16-bit data port size).

1st address is 0xA0000000, 2nd address will be 0xA0000002.

2> Please refer my above comments. 


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,913 次查看
abby
Contributor I

Hi Hui_Ma,

Thanks a lot.

Abby

0 项奖励
回复