K60 Clock Requirements

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60 Clock Requirements

跳至解决方案
1,217 次查看
Carl_7
Contributor I

I am configuring my board to use an external 25MHz crystal for the main clock. Is it absolutlely necessary to also have a 32kHz crystal on your board even if you are not using an RTC?

0 项奖励
回复
1 解答
964 次查看
comsosysarch
Contributor III

No. You do not need the 32k clock unless you specifically use it for some device module.

 

I've been using a custom dev board with only a 50 MHz high speed EXTAL for about 18 months no problem (well, no oscillator problems).

 

You can leave XTAL32 float, we've grounded EXTAL32 thru a 10M resistor, but I think that is just overkill for possible noise reduction, I do not believe it is required to actually do that. In fact it might be better without. I think the designer just did it so Altium would not complain it was a floating "input".

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
965 次查看
comsosysarch
Contributor III

No. You do not need the 32k clock unless you specifically use it for some device module.

 

I've been using a custom dev board with only a 50 MHz high speed EXTAL for about 18 months no problem (well, no oscillator problems).

 

You can leave XTAL32 float, we've grounded EXTAL32 thru a 10M resistor, but I think that is just overkill for possible noise reduction, I do not believe it is required to actually do that. In fact it might be better without. I think the designer just did it so Altium would not complain it was a floating "input".

 

0 项奖励
回复