K60 Clock Requirements

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 Clock Requirements

ソリューションへジャンプ
1,891件の閲覧回数
Carl_7
Contributor I

I am configuring my board to use an external 25MHz crystal for the main clock. Is it absolutlely necessary to also have a 32kHz crystal on your board even if you are not using an RTC?

0 件の賞賛
返信
1 解決策
1,638件の閲覧回数
comsosysarch
Contributor III

No. You do not need the 32k clock unless you specifically use it for some device module.

 

I've been using a custom dev board with only a 50 MHz high speed EXTAL for about 18 months no problem (well, no oscillator problems).

 

You can leave XTAL32 float, we've grounded EXTAL32 thru a 10M resistor, but I think that is just overkill for possible noise reduction, I do not believe it is required to actually do that. In fact it might be better without. I think the designer just did it so Altium would not complain it was a floating "input".

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,638件の閲覧回数
comsosysarch
Contributor III

No. You do not need the 32k clock unless you specifically use it for some device module.

 

I've been using a custom dev board with only a 50 MHz high speed EXTAL for about 18 months no problem (well, no oscillator problems).

 

You can leave XTAL32 float, we've grounded EXTAL32 thru a 10M resistor, but I think that is just overkill for possible noise reduction, I do not believe it is required to actually do that. In fact it might be better without. I think the designer just did it so Altium would not complain it was a floating "input".

 

0 件の賞賛
返信