K60 - Can I Leave Reset Pin Floating?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60 - Can I Leave Reset Pin Floating?

2,154件の閲覧回数
hworrall
Contributor I

We are designing a product that uses the K60 MPU. We are not planning to use the RESET_b pin (except for programming the MPU). Can this pin be left floating (it has internal pull up resistor) or should it be pulled high with an external resistor and or have a capacitor to 0V to protect it from EMC etc.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

2,001件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Hugh Worrall,

    We highly recommend you add the 4.7K to 10K external pull up resistor in the RESET pin, and add 0.1uf capacitor to the ground, even you don't want to use it.

Wish it helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------