K60, CDC Virtual Com example (running on the tower) and on-chip USB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K60, CDC Virtual Com example (running on the tower) and on-chip USB

ソリューションへジャンプ
1,809件の閲覧回数
RJS
Contributor I

Hello,

 

How can I extend the K60 MQX CDC Virtual Com example to use the on-chip USB port instead of the USB debug port on the Tower?

 

Thanks,

 

RJS

0 件の賞賛
返信
1 解決策
1,466件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

 

The MQX CDC examples are using the internal USB controller on-chip. The USB interface you have to use is the TWR-SER USB connector.

 

Best Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,467件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

 

The MQX CDC examples are using the internal USB controller on-chip. The USB interface you have to use is the TWR-SER USB connector.

 

Best Regards,

0 件の賞賛
返信
1,466件の閲覧回数
RJS
Contributor I

Luis,

 

Thanks!

 

It was right under my nose...

 

Now I just need to find out what is wrong with our prototype...

 

Cheers,

 

Bob.

0 件の賞賛
返信