K60, CDC Virtual Com example (running on the tower) and on-chip USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K60, CDC Virtual Com example (running on the tower) and on-chip USB

跳至解决方案
2,483 次查看
RJS
Contributor I

Hello,

 

How can I extend the K60 MQX CDC Virtual Com example to use the on-chip USB port instead of the USB debug port on the Tower?

 

Thanks,

 

RJS

0 项奖励
回复
1 解答
2,140 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

 

The MQX CDC examples are using the internal USB controller on-chip. The USB interface you have to use is the TWR-SER USB connector.

 

Best Regards,

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,141 次查看
LuisCasado
NXP Employee
NXP Employee

Hello,

 

The MQX CDC examples are using the internal USB controller on-chip. The USB interface you have to use is the TWR-SER USB connector.

 

Best Regards,

0 项奖励
回复
2,140 次查看
RJS
Contributor I

Luis,

 

Thanks!

 

It was right under my nose...

 

Now I just need to find out what is wrong with our prototype...

 

Cheers,

 

Bob.

0 项奖励
回复