K60, CDC Virtual Com example (running on the tower) and on-chip USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60, CDC Virtual Com example (running on the tower) and on-chip USB

Jump to solution
1,703 Views
RJS
Contributor I

Hello,

 

How can I extend the K60 MQX CDC Virtual Com example to use the on-chip USB port instead of the USB debug port on the Tower?

 

Thanks,

 

RJS

0 Kudos
Reply
1 Solution
1,360 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

 

The MQX CDC examples are using the internal USB controller on-chip. The USB interface you have to use is the TWR-SER USB connector.

 

Best Regards,

View solution in original post

0 Kudos
Reply
2 Replies
1,361 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

 

The MQX CDC examples are using the internal USB controller on-chip. The USB interface you have to use is the TWR-SER USB connector.

 

Best Regards,

0 Kudos
Reply
1,360 Views
RJS
Contributor I

Luis,

 

Thanks!

 

It was right under my nose...

 

Now I just need to find out what is wrong with our prototype...

 

Cheers,

 

Bob.

0 Kudos
Reply