K60 144-pin Pinout Discrepancy Data Sheet vs Solution Advisor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K60 144-pin Pinout Discrepancy Data Sheet vs Solution Advisor

Jump to solution
4,470 Views
MK_User
Contributor I

I just went through the solution advisor to get a .csv of the Signal Muxing section for the MK60DX256VMD10 part.

When going through the Solution Advisor generated mux table, I noticed that it has additional ALT's listed that the data sheet does not.

I am using the K60P144M100SF2V2 data sheet, Rev 2, 12/2012.

For example:

Solution Advisor Mux table has L9 : PTA11 : ALT5 = FBb_OE_b

The data sheet has no entry for L9 : PTA11 : ALT5.

So, which is correct?

Labels (1)
0 Kudos
Reply
1 Solution
3,747 Views
apanecatl
Senior Contributor II

The correct pinout is the one depicted in the Datasheet and Reference Manual

View solution in original post

0 Kudos
Reply
1 Reply
3,748 Views
apanecatl
Senior Contributor II

The correct pinout is the one depicted in the Datasheet and Reference Manual

0 Kudos
Reply