K40 Quick_Start_Demo problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K40 Quick_Start_Demo problem

ソリューションへジャンプ
1,641件の閲覧回数
cavebiker
Contributor V

I am new to CodeWarrior. I want to fire up the K40  Quick_Start_Demo so I can check-out the MQX RTOS and Codewarrior to see if I want to purchase it. But I cannot get the demo project to import.

 

The error:

When I get to step 29) in the TWR-K40X256 Quick Start Demo Lab Guide for MQX 3.7 Rev. 6 it tells me:

 

'29)Make sure TWR-K40X256_Quick_Start_Demo is checked, and hit Finish. Please read the instructions below for the error dialog box that will likely come up after hitting Finish.'

 

My problem is that the dialog box will not check. I click and click and nothing. Everything else up to this point has worked.

 

Has anyone else had this problem? And is there a solution?

 

Thanks 

 

Kinetis Rocks!


0 件の賞賛
返信
1 解決策
1,497件の閲覧回数
cavebiker
Contributor V

Nevermind, I just needed to do a clean first :smileyindifferent:

 

Proof once again that  to figure it out, sometimes all you have to do is ask the question.

 

Cheers

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,498件の閲覧回数
cavebiker
Contributor V

Nevermind, I just needed to do a clean first :smileyindifferent:

 

Proof once again that  to figure it out, sometimes all you have to do is ask the question.

 

Cheers

0 件の賞賛
返信