K40 Quick_Start_Demo problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K40 Quick_Start_Demo problem

跳至解决方案
1,647 次查看
cavebiker
Contributor V

I am new to CodeWarrior. I want to fire up the K40  Quick_Start_Demo so I can check-out the MQX RTOS and Codewarrior to see if I want to purchase it. But I cannot get the demo project to import.

 

The error:

When I get to step 29) in the TWR-K40X256 Quick Start Demo Lab Guide for MQX 3.7 Rev. 6 it tells me:

 

'29)Make sure TWR-K40X256_Quick_Start_Demo is checked, and hit Finish. Please read the instructions below for the error dialog box that will likely come up after hitting Finish.'

 

My problem is that the dialog box will not check. I click and click and nothing. Everything else up to this point has worked.

 

Has anyone else had this problem? And is there a solution?

 

Thanks 

 

Kinetis Rocks!


0 项奖励
回复
1 解答
1,503 次查看
cavebiker
Contributor V

Nevermind, I just needed to do a clean first :smileyindifferent:

 

Proof once again that  to figure it out, sometimes all you have to do is ask the question.

 

Cheers

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,504 次查看
cavebiker
Contributor V

Nevermind, I just needed to do a clean first :smileyindifferent:

 

Proof once again that  to figure it out, sometimes all you have to do is ask the question.

 

Cheers

0 项奖励
回复