K40: How to enter into low power modes?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K40: How to enter into low power modes?

Jump to solution
1,786 Views
BasePointer
Contributor II

Hi,

I want to measure K40's power consumption at KwikStik board while it is in various low power modes.

I read about AN4503 but the examples given in the datasheet are not compile-able for me.

Where are the example project files for AN4503? (I use KEIL IDE and C)

Thanks.

Tags (3)
0 Kudos
Reply
1 Solution
1,499 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

For Keil low power mode example, I have ported KINETIS_SC to Keil last year, and I remember it includes a low power mode demo named as "tsi_low_pwr", through it is for TWR-K60/K40/K53, but it should be a good reference for your case, you may download the project from Adding keil support for KINETIS_SC .

Hope that helps,


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,500 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Mehmet Fide,

For Keil low power mode example, I have ported KINETIS_SC to Keil last year, and I remember it includes a low power mode demo named as "tsi_low_pwr", through it is for TWR-K60/K40/K53, but it should be a good reference for your case, you may download the project from Adding keil support for KINETIS_SC .

Hope that helps,


Have a great day,
B.R
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply