K32W module availability without carrier exapansion

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K32W module availability without carrier exapansion

49,235件の閲覧回数
yagnikpokal
Contributor II

I see that design files are available for OM15069-K32W for K32W module. But while searching on the internet I came to know that it is not available on NXP or other websites.

Only for OM15080-K32W based modules with expansion board available.

Is there any chance that we got the raw module without the nxp expansion carrier board for OM15069-K32W type?

 

 

0 件の賞賛
返信
4 返答(返信)

49,195件の閲覧回数
yagnikpokal
Contributor II

Good if you give the answer as our architecture is going to be finalized.

 

 

0 件の賞賛
返信

49,220件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. Are you looking for the Design Files of OM15069, right?

You can find the Design Files in the K32W061 Manufacturing package: IOTZTB-DK006 (Design Resources section).

Or do you mean to buy the module? Please check the K32W-001-T10 on the IOTZTB-DK006  page.

Hope this helps.

 

Best Regards,

Ricardo

0 件の賞賛
返信

49,211件の閲覧回数
yagnikpokal
Contributor II

K32W module (K32W-001-T10) Is comes with a module + expansion board.

We need to create our own expansion board as we want to put this on a standard mikrobus connector. So K32W-001-T10 will not fit.

Hence, is there any possibility that we get K32W without an expansion board?

yagnikpokal_0-1633585755431.png

 

0 件の賞賛
返信

49,185件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

As you know, the module is part of our development kit, and therefore only the "complete" upgrade module (K32W-001-T10) is sold, to work with our DK6 carrier board.

You can take the Designs Files as a reference to make your own module.

 

Best Regards,

Ricardo

0 件の賞賛
返信