K32L2A USB pins as UART?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32L2A USB pins as UART?

Jump to solution
1,531 Views
bobpaddock
Senior Contributor III

 

In the K32L2A Reference Manual in the USB section, Chapter 51, 51.4.24 "USB Control Register (USBx_USBCTRL) states:

Bit 5: UART Signal Channel Select. [Tx/Rx on DP/DM or DM/DP selection.]

Bit 4: Selects USB signals to be used as UART signals. [Enables the above.]

What is this talking about?  If the USB module is not used for USB its pins can be used as a fourth UART?  There is no other mention of this UART anyplace else other than this section.

It is clearly NOT referring to the USB CDC Serial Class.

How is the baud set?  Bit format? Where to read/write data bytes etc...

As the USB Pins frequently already come out of the device, this would be a very useful debugging feature.

 

0 Kudos
Reply
1 Solution
1,445 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @bobpaddock 

Thanks for your patience, this is a error on the reference manual the K32L2A does not support this USB feature, I've already escalate this to the sopport team. If you are interested on this feature, look into the KS22 reference manual. You are correct, this feature allow simple debugging capabilities.

Let me know if you have another question.

Best Regards, Miguel.

View solution in original post

0 Kudos
Reply
4 Replies
1,496 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @bobpaddock 

Sorry for the late reply, I want to let you know that we have been investigating your case. 

Thanks for your patience, I will let you know as soon as we confirm what the issue is.

Best Regards, Miguel.

0 Kudos
Reply
1,481 Views
bobpaddock
Senior Contributor III
Thank you.
0 Kudos
Reply
1,446 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @bobpaddock 

Thanks for your patience, this is a error on the reference manual the K32L2A does not support this USB feature, I've already escalate this to the sopport team. If you are interested on this feature, look into the KS22 reference manual. You are correct, this feature allow simple debugging capabilities.

Let me know if you have another question.

Best Regards, Miguel.

0 Kudos
Reply
1,436 Views
bobpaddock
Senior Contributor III
Thank you for checking. It was the reply I was expecting.
0 Kudos
Reply