K32 PSTOPO Partial Stop Option

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K32 PSTOPO Partial Stop Option

2,564件の閲覧回数
aberger
Senior Contributor I

From The K32 RM, the SMC_STOPCTRL register controls the Partial Stop Option:

00 STOP - Normal Stop mode
01 PSTOP1 - Partial Stop with both system and bus clocks disabled
10 PSTOP2 - Partial Stop with system clock disabled and bus clock enabled

What is the difference between 0b00 (STOP) and 0b01 (PSTOP1)? What is the impact on recovery time? 

I am interested in waking from STOP on a UART edge. How fast can this happen in the various stop modes?

 

タグ(4)
0 件の賞賛
返信
4 返答(返信)

2,442件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @aberger 

There is no such data.

 

BR

Alice

0 件の賞賛
返信

2,510件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @aberger 

1) What about the part number you use? You can find power mode transition time for your chip from data sheet, for example K32L2B3x:

Alice_Yang_0-1704265459884.png

 

2)"What is the impact on recovery time? "

->>

PSTOP1 is functionally similar to Stop mode, but offers faster wake-up at the expense of
higher power consumption. Another benefit is that it keeps all of the MCG clocks
enabled, which can be useful for some of the asynchronous peripherals that can remain
functional in Stop modes.

 

BR

Alice

0 件の賞賛
返信

2,502件の閲覧回数
aberger
Senior Contributor I

Yes, I'm aware of the table that you referred to, but that just shows recovery time from STOP to RUN, and does not provide details about the Partial Stop options. You mentioned that PSTOP1 offers faster wake-up time than STOP. How does it compare with the 7.5 µs?

0 件の賞賛
返信

2,470件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @aberger 

There is no wake-up time from PSTOP1 to RUN in DS, I will confirm with internal.

 

BR

Alice

0 件の賞賛
返信