K27F-K28F USB VREG_OUT Capacitor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K27F-K28F USB VREG_OUT Capacitor

1,775 Views
etronic_arg
Contributor III

Hi,

I just want to know if VREG_OUT (pin G2) should be connected to an external output capacitor (COUT=2.2uF in datasheet) despite of it is not used to power any external circuit. I want to use USB FS with IRC48 as clock source. The microcontroller is powered by an external supply.

Thanks!

Labels (2)
0 Kudos
Reply
2 Replies

1,661 Views
mjbcswitzerland
Specialist V

Hi

The capacitor is used to stabilise the low dropout regulator used to supply stable USB PHY power supply. This means that if FS USB is used it must be connected. If not, USB will not work.
Make sure that the capacitor type used fulfills the low ESD requirements as specified in the manual and data sheet.

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

1,661 Views
etronic_arg
Contributor III

Thank you. Just as I thought! I didn't realize to put it in my board... 

0 Kudos
Reply