K27F-K28F USB VREG_OUT Capacitor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K27F-K28F USB VREG_OUT Capacitor

1,791件の閲覧回数
etronic_arg
Contributor III

Hi,

I just want to know if VREG_OUT (pin G2) should be connected to an external output capacitor (COUT=2.2uF in datasheet) despite of it is not used to power any external circuit. I want to use USB FS with IRC48 as clock source. The microcontroller is powered by an external supply.

Thanks!

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

1,677件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The capacitor is used to stabilise the low dropout regulator used to supply stable USB PHY power supply. This means that if FS USB is used it must be connected. If not, USB will not work.
Make sure that the capacitor type used fulfills the low ESD requirements as specified in the manual and data sheet.

Regards

Mark

[uTasker project developer for Kinetis and i.MX RT]

1,677件の閲覧回数
etronic_arg
Contributor III

Thank you. Just as I thought! I didn't realize to put it in my board... 

0 件の賞賛
返信