K27 VDIO and VAIO specification

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K27 VDIO and VAIO specification

跳至解决方案
2,034 次查看
masahirokiniwa
Contributor IV

Hi,

Could you tell me VDIO(Digital input voltage) and VAIO(Analog input voltage) for Kinetis K27?

Are their specification VDD+0.3V same as K26?

Best regards,

M.KIniwa

标签 (1)
0 项奖励
回复
1 解答
1,926 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Masahiro,

I think the answer is yes, the VDIO(Digital input voltage pin) is from -0.3 to VDD+0.3, VAIO( Analog input voltage pin) is from -0.3 to VDD+0.3.

Hope it can help you

BR

XiangJun Rong

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,927 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Masahiro,

I think the answer is yes, the VDIO(Digital input voltage pin) is from -0.3 to VDD+0.3, VAIO( Analog input voltage pin) is from -0.3 to VDD+0.3.

Hope it can help you

BR

XiangJun Rong

0 项奖励
回复