K27 VDIO and VAIO specification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K27 VDIO and VAIO specification

Jump to solution
2,029 Views
masahirokiniwa
Contributor IV

Hi,

Could you tell me VDIO(Digital input voltage) and VAIO(Analog input voltage) for Kinetis K27?

Are their specification VDD+0.3V same as K26?

Best regards,

M.KIniwa

Labels (1)
0 Kudos
Reply
1 Solution
1,921 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Masahiro,

I think the answer is yes, the VDIO(Digital input voltage pin) is from -0.3 to VDD+0.3, VAIO( Analog input voltage pin) is from -0.3 to VDD+0.3.

Hope it can help you

BR

XiangJun Rong

View solution in original post

0 Kudos
Reply
1 Reply
1,922 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Masahiro,

I think the answer is yes, the VDIO(Digital input voltage pin) is from -0.3 to VDD+0.3, VAIO( Analog input voltage pin) is from -0.3 to VDD+0.3.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply