K27 VDIO and VAIO specification

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K27 VDIO and VAIO specification

ソリューションへジャンプ
2,515件の閲覧回数
masahirokiniwa
Contributor IV

Hi,

Could you tell me VDIO(Digital input voltage) and VAIO(Analog input voltage) for Kinetis K27?

Are their specification VDD+0.3V same as K26?

Best regards,

M.KIniwa

ラベル(1)
0 件の賞賛
返信
1 解決策
2,407件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Masahiro,

I think the answer is yes, the VDIO(Digital input voltage pin) is from -0.3 to VDD+0.3, VAIO( Analog input voltage pin) is from -0.3 to VDD+0.3.

Hope it can help you

BR

XiangJun Rong

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,408件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Masahiro,

I think the answer is yes, the VDIO(Digital input voltage pin) is from -0.3 to VDD+0.3, VAIO( Analog input voltage pin) is from -0.3 to VDD+0.3.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信