K22FN512X Flashloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22FN512X Flashloader

ソリューションへジャンプ
2,148件の閲覧回数
antoinee
Contributor I

Hi,

I would like programming the microcontroller MK22FN512VLH12 in flashloader method (With FSL_Kinetis_Bootloader_1_1_0).

What are the pins to be connected to the computer?

thank .

Antoine

0 件の賞賛
返信
1 解決策
2,020件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

You can check the pin information in the specific device reference manual. For the K22 you can see the Flash Loader chapter; the image below shows the pin table for the Flashloader:

k22boot.jpg

If you are using the FRDM-K22F you can use the Virtual COM port connected through the OpenSDA connector that uses theUART1 module: PTE0 and PTE1.

Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,020件の閲覧回数
antoinee
Contributor I

Hi,

Thank.:smileyhappy:

0 件の賞賛
返信
2,021件の閲覧回数
adriancano
NXP Employee
NXP Employee

Hi,

You can check the pin information in the specific device reference manual. For the K22 you can see the Flash Loader chapter; the image below shows the pin table for the Flashloader:

k22boot.jpg

If you are using the FRDM-K22F you can use the Virtual COM port connected through the OpenSDA connector that uses theUART1 module: PTE0 and PTE1.

Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信