K22FN512X Flashloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K22FN512X Flashloader

Jump to solution
2,321 Views
antoinee
Fresh Out Contributor

Hi,

I would like programming the microcontroller MK22FN512VLH12 in flashloader method (With FSL_Kinetis_Bootloader_1_1_0).

What are the pins to be connected to the computer?

thank .

Antoine

0 Kudos
Reply
1 Solution
2,193 Views
adriancano
NXP Employee
NXP Employee

Hi,

You can check the pin information in the specific device reference manual. For the K22 you can see the Flash Loader chapter; the image below shows the pin table for the Flashloader:

k22boot.jpg

If you are using the FRDM-K22F you can use the Virtual COM port connected through the OpenSDA connector that uses theUART1 module: PTE0 and PTE1.

Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,193 Views
antoinee
Fresh Out Contributor

Hi,

Thank.:smileyhappy:

0 Kudos
Reply
2,193 Views
adriancano
NXP Employee
NXP Employee

Hi,

You can check the pin information in the specific device reference manual. For the K22 you can see the Flash Loader chapter; the image below shows the pin table for the Flashloader:

k22boot.jpg

If you are using the FRDM-K22F you can use the Virtual COM port connected through the OpenSDA connector that uses theUART1 module: PTE0 and PTE1.

Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply