K22FN512X Flashloader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

K22FN512X Flashloader

跳至解决方案
2,177 次查看
antoinee
Contributor I

Hi,

I would like programming the microcontroller MK22FN512VLH12 in flashloader method (With FSL_Kinetis_Bootloader_1_1_0).

What are the pins to be connected to the computer?

thank .

Antoine

0 项奖励
回复
1 解答
2,049 次查看
adriancano
NXP Employee
NXP Employee

Hi,

You can check the pin information in the specific device reference manual. For the K22 you can see the Flash Loader chapter; the image below shows the pin table for the Flashloader:

k22boot.jpg

If you are using the FRDM-K22F you can use the Virtual COM port connected through the OpenSDA connector that uses theUART1 module: PTE0 and PTE1.

Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,049 次查看
antoinee
Contributor I

Hi,

Thank.:smileyhappy:

0 项奖励
回复
2,050 次查看
adriancano
NXP Employee
NXP Employee

Hi,

You can check the pin information in the specific device reference manual. For the K22 you can see the Flash Loader chapter; the image below shows the pin table for the Flashloader:

k22boot.jpg

If you are using the FRDM-K22F you can use the Virtual COM port connected through the OpenSDA connector that uses theUART1 module: PTE0 and PTE1.

Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复