K22 programming problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K22 programming problem

ソリューションへジャンプ
1,687件の閲覧回数
kaarthichandras
Contributor II

hi,

I'm using MK22DX256VLF5 MCU package ,how  to convert .elf file into .s19 file format  ?

note :i am using codewarrior development studio 10.6

ラベル(2)
0 件の賞賛
返信
1 解決策
1,587件の閲覧回数
BlackNight
NXP Employee
NXP Employee

In CodeWarrior you have the option to 'generate S-Record', see S-Record, Intel Hex and Binary Files | MCU on Eclipse or see this: S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse .

Other than that, you can use one of the many tools to convert files. I'm using the Srecord utility, see Converting Binary Files to Intel Hex Format with the SRecord Tool | MCU on Eclipse  (works the same for S19).

I hope this helps,

Erich

PS: in MCUXpresso IDE it is done like this: MCUXpresso IDE: S-Record, Intel Hex and Binary Files | MCU on Eclipse  and in KDS it is like this:  Binary (and S19) Files for the mbed Bootloader with Eclipse and GNU ARM Eclipse Plugins | MCU on Ecl... 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,587件の閲覧回数
BlackNight
NXP Employee
NXP Employee

In CodeWarrior you have the option to 'generate S-Record', see S-Record, Intel Hex and Binary Files | MCU on Eclipse or see this: S-Record Generation with gcc for ARM/Kinetis | MCU on Eclipse .

Other than that, you can use one of the many tools to convert files. I'm using the Srecord utility, see Converting Binary Files to Intel Hex Format with the SRecord Tool | MCU on Eclipse  (works the same for S19).

I hope this helps,

Erich

PS: in MCUXpresso IDE it is done like this: MCUXpresso IDE: S-Record, Intel Hex and Binary Files | MCU on Eclipse  and in KDS it is like this:  Binary (and S19) Files for the mbed Bootloader with Eclipse and GNU ARM Eclipse Plugins | MCU on Ecl... 

0 件の賞賛
返信