K22 Custom board bring up issue - PE Multilink and KDS2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

K22 Custom board bring up issue - PE Multilink and KDS2.0

1,192 次查看
SaravanaPandian
Contributor I

Hi,

  We are bringing up a custom K22 based board. We are using P&E Multilink Rev.C with KDS 2.0 and initially we could program the K22 in SWD mode. But after a few tries, it stopped working and says "Can not enter background mode.

Unable to initialize PEDebug.

PE-ERROR: Failed to Initialize Target".

  We have done all the steps mentioned by Amit/Jose in thread (https://community.freescale.com/thread/318552) but still could not make it communicate. Even JTAG mode is not working.

 

  On analysis, we find that the RESET is occurring continuously (as we might have erased flash, causing WDRST).  When we connect with debugger (or erase flash) and it is sending the JTAG to SWD pattern, we observe the pattern as in the picture. Red is SWDCLK and yellow is SWDDIO. Frequency is just 100KHz.

K22_SWDDIO_Issue_s.jpg

 

  Only for the first 50 clocks and 79E7h pattern the SWDDIO is driven at 3.3 V whereas after that the high level is struck at 1.6V only. We tried increasing the SWDDIO pull-up to 1K, but with no effect. Is this a cause for concern?

 

  The same debugger works fine with our custom KL25 based board with full voltage SWDDIO swing.

 

  Looking forward for support from the community.

Thanks and Regards,

Saravana Pandian

0 项奖励
回复
1 回复

898 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Saravana Pandian,

from your description, you use "P&E Multilink Rev.C", is it http://www.pemicro.com/products/product_viewDetails.cfm?product_id=33  ?

"P&E Multilink is not for Kinetis.

to work with Kinetis, we use USB Multilink Universal

http://www.pemicro.com/products/product_viewDetails.cfm?product_id=15320137

or USB Multilink Universal FX

P&E Microcomputer Systems - USB Multilink Universal FX - USB Multilink Universal FX All-In-One Devel...

are you sure you use the correct emulator?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复