K21F How to use the internal oscillator

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K21F How to use the internal oscillator

6,869 Views
黃佑煊
Contributor II

HI !

How to use the internal oscillator ?

Using the internal oscillator, the oscillator to add it?

Labels (1)
0 Kudos
Reply
8 Replies

6,733 Views
jeremyzhou
NXP Employee
NXP Employee

Hi

附件是关于Kineis 系统时钟的介绍,你可以参考一下。


Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

6,733 Views
黃佑煊
Contributor II

HI !

請求更多協助,有關於K21F 內部振盪器的使用.

0 Kudos
Reply

6,733 Views
jeremyzhou
NXP Employee
NXP Employee

Hi

妳的問題範圍太廣了,單單用回復,我想是不能包括所有內容的,建議妳最好去看參考手冊中關於OSC和MCG章節的內容。

还有妳能不能具體告訴我,想用內部參考時鐘生成什麽樣的時鐘模式,這樣我就可以告訴妳具體的實現方式啊!!
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

6,733 Views
黃佑煊
Contributor II

HI !

我想使用內部振盪器,逹到core 120MHz 謝謝~ 

0 Kudos
Reply

6,733 Views
cutworth
NXP Employee
NXP Employee

Your question is still not clear. I suppose you wish to use internal slow IRC (32kHz) to generate 120MHz core clock, right? If so, then this is not possible. Using internal clock, you can just use FLL which has maximum output of 100MHz. You will need to use PLL for 120MHz and PLL requires external clock, for external clock, you will need to use the internal oscillator when connecting a crystal.

Hao

0 Kudos
Reply

6,733 Views
黃佑煊
Contributor II

HI !

如何用內部振盪器 使core 100MHz

0 Kudos
Reply

6,733 Views
cutworth
NXP Employee
NXP Employee

You can use FLL in MCG module to achieve 100MHz core clock with internal 32kHz OSC. Configure MCG_C4.

0 Kudos
Reply

6,733 Views
cutworth
NXP Employee
NXP Employee

Hi,

Which part for internal OSC you want to know? I suppose you are referring to the main oscillator instead of RTC OSC, right?

For the main oscillator, there are different oscillator modes, low frequency, high gain, low power, etc. And you can configure the exact mode used with MCG_C2 register.

For the different mode, the external circuit connection is also different, please refer to OSC chapter for detailed information.

Hao

0 Kudos
Reply