K21DN512 USB1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K21DN512 USB1.1

1,322 Views
fredfu
NXP Employee
NXP Employee

Hi,

   My customer--Fujian Landi want to use low speed USB device for K21, now USB can't work well. i tried the customer's problem,  I pull up 1.5K resistor in D-, and run KSDK1.2.0 USB HID device example in TWR-K21D50M,PC can't recognize the device. I read the K21DN512 RM, and found RM only mention OTG supports FS device. K21DN512 can support LOW SPEED device? and How to run LOW SPEED USB examples? Thanks.

pastedImage_0.png

Best Regards,

Fred Fu

Labels (2)
0 Kudos
Reply
1 Reply

1,174 Views
isaacavila
NXP Employee
NXP Employee

Hello Yanrong Fu,

As you may notice, Reference manual says Low Speed functionality is only available when board is configured as Host (That is why, in next point it says that USB transceiver includes internal pulldowns on D+ and D- lines for host mode functionality). So basically, this MCU does not support Low Speed when configured as Device.

Sorry for inconvenience it may cause!

Best Regards,

Isaac

----------------------------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply