[K20D50M]: Is USB Device D+ High in VLPS Mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[K20D50M]: Is USB Device D+ High in VLPS Mode?

Jump to solution
1,716 Views
huishao2
Contributor IV

Hi-

I have a question regarding D+ status when K20D50 is in VLPS low power mode:

is it still high when K20 enters stop mode?

Thanks!

Hui

Labels (2)
0 Kudos
Reply
1 Solution
1,597 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Hui,

According to the reference manual, when the USBOTG module enter the low-power mode, its status will move to the Suspend mode.

While in the Suspend state, a device must continue to provide power to its D+ ( full/high-speed ) or D- ( low-speed ) pull up resistor to maintain an idle so that the upstream hub can maintain the correct connectivity status for the device.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,598 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Hui,

According to the reference manual, when the USBOTG module enter the low-power mode, its status will move to the Suspend mode.

While in the Suspend state, a device must continue to provide power to its D+ ( full/high-speed ) or D- ( low-speed ) pull up resistor to maintain an idle so that the upstream hub can maintain the correct connectivity status for the device.

Hope it helps.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply