K20D50: how to enable USB VBus charging to USB device?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K20D50: how to enable USB VBus charging to USB device?

2,300件の閲覧回数
huishao2
Contributor IV

Hi-

I am using MK20DX128VFM5 and trying to build up a USB CDC host board to drive the enumeration and charging of a CDC device. My custom board is receiving +12V DC from power source and I expect the charging current to be around 400mA.

Question is, how can I make VBus of K20 to output current above for charging purpose? I see from user manual there is a USB Voltage Regulator inside k20, but its output is only 120mA.

Is there a reference design available for such case?

thanks!

Hui

タグ(1)
3 返答(返信)

2,034件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check below DC-DC circuit for 12V transfer to 5V:

power.png

The USB VBUS can use this 5V source.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,034件の閲覧回数
huishao2
Contributor IV

Hi Hui,

Thank you so much for the detailed circuitry design. One more question regarding this design, can I short 5V_EXT directly to my K20's VBUS? Will it reversely charge my USB host?

Thanks!

Hui

0 件の賞賛
返信

2,034件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

You can directly connect 5V_EXT to USB VBUS to power external USB device.

It also can provide power to the USB host (K20) board.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------