K10 using I2S MIC.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K10 using I2S MIC.

1,593 Views
c393
Contributor II

I have a K10P144M120 design. I have a I2S MIC connected to I2S1_RXD0, I2S1_BCLK and I2S1_RX_FS. Can I configure the SAI module for receive only? Do I have to configure the transmit?  It appears that the RX BCLK source is from the transmit BCLK. Can I configure the transmit but do not configure the I/O pins? 

Tags (3)
0 Kudos
Reply
1 Reply

1,428 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Dennis

Yes, you can configure it as receiver only. For your last question, I cannot understand it clearly. Would you please to make me clear? Thanks.

Best Regards

Paul

0 Kudos
Reply