K10 reference manual

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K10 reference manual

2,071件の閲覧回数
billnd
Contributor IV

I'm working on a deign that uses a MK10DN512VLL10 device. The reference manual on the Freescale website is K10P100M100SF2V2RM, but this is dated 2012 and marked up (in big red letters) as preliminary. Should this concern me? Is there ever likely to be a update?

Cheers in advance,

Bill

タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,876件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi billnd,

The K10P100M100SF2V2RM on our web which shows "Rev. 2 Jun 2012" is the newest Reference Manual for your MCU.

I have not found the newer versions.

If you meet problem , you can easily post question in our community.

Best Regards,

Binbin

0 件の賞賛
返信

1,876件の閲覧回数
billnd
Contributor IV

Thanks for the reply Binbin.

You are correct, Rev. 2 June 2012 is the latest one on your website. I've not found any problems with it, but the fact that it is marked as "preliminary" makes me a little nervous. "preliminary" suggests that there is going to be a "final" version at some point, but I'm guessing this is not the case.

Cheers,

Bill

0 件の賞賛
返信