K10 board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K10 board

1,934件の閲覧回数
Bolt
Contributor I

Does anyone know a board with the k10 of 48 pins?

Thanks in advance

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,834件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Javi,

What do you mean? A third party board using the K10 in 48 pins to buy as finished board?

Best Regards,

Luis

0 件の賞賛
返信

1,834件の閲覧回数
Bolt
Contributor I

Hi Luis,

No, it's just to go doing the software for the same part as in our project.

Thanks

0 件の賞賛
返信

1,834件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hi Javi,

Ok, I don't know any board with K10, I am not sure about what K10 you need (50, 72, 100 Mhz,...) But the code you write at the same speed grade Kinetis (K60, K20,..) will be 100% compatible if you use the same peripherals that K10 has. But the GPIOMUX will have to be tuned for your custom harware with K10.

Perhaps anyone knows in the community about an available board.

Luis,

0 件の賞賛
返信