K10 VREFH/VREFL Input Capacitance (ADC Problem)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K10 VREFH/VREFL Input Capacitance (ADC Problem)

2,459件の閲覧回数
ttocsmi
Contributor I

Hello,

Has anyone experienced a similar problem with ADC inputs on the K10?  The steady-state value in the center of the display is the voltage I'm trying to read.  The ADC is reporting the value at the bottom of the spikes - in this case ~79 mV too low.  Perhaps I need more capacitance at the input, or less capacitance on the VREFH/L pins?  Any advice will be appreciated.

Thanks.

temp input.jpg

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 返信

2,109件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Scott,

I'd like to suggest that the Vrefh should be stable voltage as possible, and please refer to AN4373 which about how to get the best performance of ADC.

I've also included the application note with this reply and check it.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信