K10 VREFH/VREFL Input Capacitance (ADC Problem)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K10 VREFH/VREFL Input Capacitance (ADC Problem)

2,490 Views
ttocsmi
Contributor I

Hello,

Has anyone experienced a similar problem with ADC inputs on the K10?  The steady-state value in the center of the display is the voltage I'm trying to read.  The ADC is reporting the value at the bottom of the spikes - in this case ~79 mV too low.  Perhaps I need more capacitance at the input, or less capacitance on the VREFH/L pins?  Any advice will be appreciated.

Thanks.

temp input.jpg

Labels (1)
0 Kudos
Reply
1 Reply

2,140 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Scott,

I'd like to suggest that the Vrefh should be stable voltage as possible, and please refer to AN4373 which about how to get the best performance of ADC.

I've also included the application note with this reply and check it.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply