Hi Howard Lehman,
1. About your case 00262135
After checking it, I find our two colleagues already give you a lot of suggestions, do you try it on your side?
I find my colleague reply you on 3/6/2020, but it seems you didn't give any feedback, they still waiting for your reply, could you tell me why you don't follow it any more?
2. Talkback to your question
You mentioned: I’m dealing with a family of 10 parts installed on assemblies, at least 3 have exhibited the condition.
Do you mean, other 7 boards are working perfectly, with the same code, the same board design, the same K10 chip, right? Just 3 boards meet the overheat problems?
Could you please tell me your K10 LQ12 detail part number, and your maskset?
With the 3 issue boards, do you try the case engineer suggested way:
load a simple project that only set one gpio,with this you can check if the device is getting hot or not, if not then you can add
other module like uart, and continue the test Also can you check if there is not any manufacturing issue,like a solder short, missing part…
If you can not perform a swap test, then I believe the best option to find the problem is testing module by module
Any updated test result?
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------