K02P64M100SFARM can i put vref 1.2 on an adc input pin?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

K02P64M100SFARM can i put vref 1.2 on an adc input pin?

754件の閲覧回数
johnsmith3
Contributor I

Hi all,

can i put vref 1.2 on an adc input pin on a k02 ?

nothing there in the K02F Sub-Family Reference Manual....

regards,

ラベル(1)
0 件の賞賛
返信
1 返信

658件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

You can put the vref 1.2v on an ADC input pin. But it need to be connected from outside of the MCU, due to the vref 1.2v is not on the list of "3.7.1.3 ADCx Connections/Channel Assignment" in K02P64M100SFARM).

The ADC input voltage must not higher than the voltage of ADC reference. See the "3.6.1.1 16-bit ADC operating conditions" in K02P64M100SFA.

VADIN.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信