K02P64M100SFARM can i put vref 1.2 on an adc input pin?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K02P64M100SFARM can i put vref 1.2 on an adc input pin?

1,131 Views
johnsmith3
Contributor I

Hi all,

can i put vref 1.2 on an adc input pin on a k02 ?

nothing there in the K02F Sub-Family Reference Manual....

regards,

Labels (1)
0 Kudos
Reply
1 Reply

1,035 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

You can put the vref 1.2v on an ADC input pin. But it need to be connected from outside of the MCU, due to the vref 1.2v is not on the list of "3.7.1.3 ADCx Connections/Channel Assignment" in K02P64M100SFARM).

The ADC input voltage must not higher than the voltage of ADC reference. See the "3.6.1.1 16-bit ADC operating conditions" in K02P64M100SFA.

VADIN.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
---------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply