Issues compiling the TWRK40X256QSDLAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Issues compiling the TWRK40X256QSDLAB

1,890件の閲覧回数
reddeuce
Contributor II

Has anyone been able to get the TWR-K40X256 demo code to compile using CW10.3 and MQX3.7?  I have a new TWR-K40X256 kit and have been able to successfully get through the quick start demo lab guide (TWRK40X256QSDLAB) up to step 38, where you have to build the demo code project. The build fails with 7 errors:

Description Resource Path Location Type

mingw32-make: *** [Sources/adc/ADC_Task_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/slcd/SLCD_Task_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/slcd/twrpi_slcd_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/tsi/tsi_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/usb/mouse_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/usb/usb_descriptor_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

while parsing option '-i' TWR-K40X256_Quick_Start_Demo    C/C++ Problem

Can anyone give me some hints what to try to get this demo to compile?

Thanks.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,722件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

Did you try using CW 10.1???

BR

Sol

0 件の賞賛
返信

1,722件の閲覧回数
reddeuce
Contributor II

Hello -

No. I don't have CW 10.1. I didn't see it available for download any longer.  I'm trying to use the newest tools, so I'd really like to know what to do to get the code to compile on CW 10.3.

Regards,

Mike Cox

0 件の賞賛
返信