Issues compiling the TWRK40X256QSDLAB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issues compiling the TWRK40X256QSDLAB

2,013 次查看
reddeuce
Contributor II

Has anyone been able to get the TWR-K40X256 demo code to compile using CW10.3 and MQX3.7?  I have a new TWR-K40X256 kit and have been able to successfully get through the quick start demo lab guide (TWRK40X256QSDLAB) up to step 38, where you have to build the demo code project. The build fails with 7 errors:

Description Resource Path Location Type

mingw32-make: *** [Sources/adc/ADC_Task_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/slcd/SLCD_Task_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/slcd/twrpi_slcd_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/tsi/tsi_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/usb/mouse_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

mingw32-make: *** [Sources/usb/usb_descriptor_c.obj] Error 1 TWR-K40X256_Quick_Start_Demo    C/C++ Problem

while parsing option '-i' TWR-K40X256_Quick_Start_Demo    C/C++ Problem

Can anyone give me some hints what to try to get this demo to compile?

Thanks.

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,845 次查看
soledad
NXP Employee
NXP Employee

Hello,

Did you try using CW 10.1???

BR

Sol

0 项奖励
回复

1,845 次查看
reddeuce
Contributor II

Hello -

No. I don't have CW 10.1. I didn't see it available for download any longer.  I'm trying to use the newest tools, so I'd really like to know what to do to get the code to compile on CW 10.3.

Regards,

Mike Cox

0 项奖励
回复