Is there source code available for blhost?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there source code available for blhost?

跳至解决方案
10,516 次查看
brycelembke
Contributor III

For automated updates to my K10 microcontroller my host must be Linux.I want to rebuild the blhost application for Linux since the only executable Freescale provides seems to be for Windows.

标记 (3)
1 解答
8,282 次查看
adriancano
NXP Employee
NXP Employee

Hi,

Are you referring to the KBOOT blhost? If yes the source code is available within the KBOOT package following the path <install_folder>\FSL_Kinetis_Bootloader_1_0_2\validation\blhost


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
9 回复数
8,282 次查看
donwilley
Contributor II

Any chance the README file mentioned earlier could be attached or quoted here?

0 项奖励
回复
8,282 次查看
sensenthuran
Contributor IV

hi brycelembke  

Did you compile blhost NXP_Kinetis_Bootloader_2_0_0? They have the make file but we need to git rid of udev as we need UART not USB.

Thanks

0 项奖励
回复
8,282 次查看
thomasschmid
Contributor II

Hi,

Have you ever succeeded in writing a Linux version of this tool? I would be highly interested in it too.

0 项奖励
回复
8,282 次查看
brycelembke
Contributor III

Yes, we did get this to build under Linux. Follow the README.txt that I put there (you will need to install CMAKE). This works with serial, I haven't tried it with USB (and may have even disabled it).

http://d3.dtectsystems.net/FSL_Kinetis_Bootloader_Linux.tgzhttp://d3.dtectsystems.net/download/FSL_Kinetis_Bootloader_Linux.tgz

8,282 次查看
rtoma
Contributor III

Links are dead now. Is there a way to compile blhost?

0 项奖励
回复
8,282 次查看
benjaminchang
Contributor V

Hi Bryce,

We are now facing the same Linux tool issue.

Tried to download your .tgz file, but seems not available now.

Can you share the file again?

Thank you!

Benjamin

0 项奖励
回复
8,282 次查看
brycelembke
Contributor III

The first link I posted was dead. Use the second link.

0 项奖励
回复
8,282 次查看
brycelembke
Contributor III

Too many links, use the second link

0 项奖励
回复
8,283 次查看
adriancano
NXP Employee
NXP Employee

Hi,

Are you referring to the KBOOT blhost? If yes the source code is available within the KBOOT package following the path <install_folder>\FSL_Kinetis_Bootloader_1_0_2\validation\blhost


Hope this information can help you.

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复