Is there any difference in the conversion time depending on the AD conversion mode?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is there any difference in the conversion time depending on the AD conversion mode?

ソリューションへジャンプ
2,469件の閲覧回数
rs__zen
Contributor I

Hi.

I'm using the MKE14F.

In ADC, I can choose conversion mode about  8, 10, or 12 bits.

So, if I choose the 8bit conversion mode, it is the more fast conversion than 12bit mode?

Or, are there same conversion time about 8, 10, 12bits? 

Please tell me.

Thank you very much.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,464件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Yes. Please read the "37.5.4.5 Sample time and total conversion time" of KE1XFP100M168SF0RM.

37.5.4.5 Sample time and total conversion time.png

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,465件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Yes. Please read the "37.5.4.5 Sample time and total conversion time" of KE1XFP100M168SF0RM.

37.5.4.5 Sample time and total conversion time.png

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信
2,454件の閲覧回数
rs__zen
Contributor I

Dear Robin

Thank you for your answer.

I'll read this section.

Best regards.

0 件の賞賛
返信