Is there any difference in the conversion time depending on the AD conversion mode?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there any difference in the conversion time depending on the AD conversion mode?

Jump to solution
2,471 Views
rs__zen
Contributor I

Hi.

I'm using the MKE14F.

In ADC, I can choose conversion mode about  8, 10, or 12 bits.

So, if I choose the 8bit conversion mode, it is the more fast conversion than 12bit mode?

Or, are there same conversion time about 8, 10, 12bits? 

Please tell me.

Thank you very much.

Labels (1)
0 Kudos
Reply
1 Solution
2,466 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Yes. Please read the "37.5.4.5 Sample time and total conversion time" of KE1XFP100M168SF0RM.

37.5.4.5 Sample time and total conversion time.png

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

View solution in original post

0 Kudos
Reply
2 Replies
2,467 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Yes. Please read the "37.5.4.5 Sample time and total conversion time" of KE1XFP100M168SF0RM.

37.5.4.5 Sample time and total conversion time.png

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 Kudos
Reply
2,456 Views
rs__zen
Contributor I

Dear Robin

Thank you for your answer.

I'll read this section.

Best regards.

0 Kudos
Reply