Is there any difference in the conversion time depending on the AD conversion mode?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Is there any difference in the conversion time depending on the AD conversion mode?

跳至解决方案
1,644 次查看
rs__zen
Contributor I

Hi.

I'm using the MKE14F.

In ADC, I can choose conversion mode about  8, 10, or 12 bits.

So, if I choose the 8bit conversion mode, it is the more fast conversion than 12bit mode?

Or, are there same conversion time about 8, 10, 12bits? 

Please tell me.

Thank you very much.

标签 (1)
0 项奖励
回复
1 解答
1,639 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Yes. Please read the "37.5.4.5 Sample time and total conversion time" of KE1XFP100M168SF0RM.

37.5.4.5 Sample time and total conversion time.png

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,640 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Yes. Please read the "37.5.4.5 Sample time and total conversion time" of KE1XFP100M168SF0RM.

37.5.4.5 Sample time and total conversion time.png

 

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 项奖励
回复
1,629 次查看
rs__zen
Contributor I

Dear Robin

Thank you for your answer.

I'll read this section.

Best regards.

0 项奖励
回复