Is there a header file BME.h

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is there a header file BME.h

Jump to solution
4,772 Views
jun1
Contributor V

Hi.

I am using KM34.

Is there a header file when using the Bit Manipulation Engine (BME)?
#define BME_AND (ADDR) ????

0 Kudos
Reply
1 Solution
4,742 Views
bobpaddock
Senior Contributor III

I attached what you are looking for.

What I'd like to know is where to find?:

"Bit Manipulation engine Block Guide v0.3."

that that file was created from.

The KE04 driver library has a BME demo with code:

https://community.nxp.com/t5/Kinetis-Microcontrollers/BME-h/m-p/945486

I never understand why NXP makes this stuff so hard to find...

View solution in original post

0 Kudos
Reply
3 Replies
4,743 Views
bobpaddock
Senior Contributor III

I attached what you are looking for.

What I'd like to know is where to find?:

"Bit Manipulation engine Block Guide v0.3."

that that file was created from.

The KE04 driver library has a BME demo with code:

https://community.nxp.com/t5/Kinetis-Microcontrollers/BME-h/m-p/945486

I never understand why NXP makes this stuff so hard to find...

0 Kudos
Reply
4,758 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @jun1 ,

Can you please help me by providing more information regarding your request.

Are you using and SDK example for the KM34?

TWR-KM34Z75M 

0 Kudos
Reply
4,748 Views
jun1
Contributor V

Hi.

thank you for your reply.
SDK uses "SDK_2_10_0_MKM34Z256xxx7". Attach the content list.
So, is there an API to access BME to the drivers in this?
I don't think fsl_gpio.c is using BME, but if you are using BME, please tell me what kind of API it will be.
Thank you.

0 Kudos
Reply