Is anyone using std::chrono with a K28F?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is anyone using std::chrono with a K28F?

1,583 次查看
edw8
Contributor III

I'm having a hard time getting anything better than a 1 second resolution on a sample c++ project exercising a timer class based on std::chrono::system_clock. This is on a C++ project based on SDK 2.2 using MCUXpresso IDE 10.0.2

0 项奖励
回复
1 回复

1,381 次查看
egoodii
Senior Contributor III

I can't be any help with the C++ class functions, but I can say that the 'fundamental RTC time register' in Kinetis is 'seconds'.  Now, that being said, as long as your setup isn't using the Time Compensation functions of the hardware, then the RTC system will be running 32768 counts per each said second via the Time Prescale Register, and you can read that and divide by 32.768 (for instance) to get milliseconds, or multiply by 30.517578125 (15625/512) to get microseconds.

Note that the RTC hardware is built of 'slow ripple counter' blocks, and it is necessary to 'read twice and compare' to insure a valid read.  See also:

RTC and Sub second Time 

0 项奖励
回复