Is NXP Touch Software compatible with the Kenetis SDK 2.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is NXP Touch Software compatible with the Kenetis SDK 2.0

1,580 次查看
davidfindlay
Contributor III

I am about to start a project with 3 cap touch buttons. Each button has it's own trace. I really have 2 questions. Do I need to use the NXP touch software to implement simple buttons? It seems to be geared more towards sliders and number pads.

The second question is whether or not that library is compatible with the newer SDK 2.0.

Thanks

0 项奖励
回复
3 回复数

1,323 次查看
miduo
NXP Employee
NXP Employee

Hi,

Yes, it is supported by the SDK 2.0.  Here is a useful start guide on this regard:https://community.nxp.com/docs/DOC-329432

0 项奖励
回复

1,323 次查看
davidfindlay
Contributor III

Please see the following screenshot. The touch software seems to insist on SDK V 1.2 which I can not even figure out how to obtain anymore. I can only get 2.0 and 1.3. Both of these don't work when I attempt to install the library.

pastedImage_1.png

0 项奖励
回复

1,323 次查看
davidfindlay
Contributor III

Yes but this guide clearly seems to imply you need the KSDK 1.2. And after attempting to run the installer it seems to be insisting on it. I get the following error.

"The selected KSDK folder doesn't content Freescale KSDK 1.2"

0 项奖励
回复