Is NXP Touch Software compatible with KL26Z?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is NXP Touch Software compatible with KL26Z?

ソリューションへジャンプ
2,379件の閲覧回数
diegovalladolid
Contributor II

I am experimenting some problems with my implementation of the TSI using the KSDK (tsi_v4.h/.c). It seems the sensitivity of the capacitive sensors vary with the input voltage and I am thinking of using the NXP Touch Software to check if that library solves my problems.

0 件の賞賛
返信
1 解決策
2,290件の閲覧回数
diegovalladolid
Contributor II

After some research I see that the NXP Touch Library 2.0.0 is not compatible with KL26 despite the manual reference (NT20RM) it indeed states it is. The reason is that the library only implements the management of the TSI v5.

So here comes another question, will NXP Touch Library be compatible with KL Series in a near future?

元の投稿で解決策を見る

2 返答(返信)
2,290件の閲覧回数
fangli
NXP Employee
NXP Employee

Hi,

There has no any plan that Touch Library will support the KL Series. Sorry.

2,291件の閲覧回数
diegovalladolid
Contributor II

After some research I see that the NXP Touch Library 2.0.0 is not compatible with KL26 despite the manual reference (NT20RM) it indeed states it is. The reason is that the library only implements the management of the TSI v5.

So here comes another question, will NXP Touch Library be compatible with KL Series in a near future?