Is NXP Touch Software compatible with KL26Z?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is NXP Touch Software compatible with KL26Z?

Jump to solution
2,409 Views
diegovalladolid
Contributor II

I am experimenting some problems with my implementation of the TSI using the KSDK (tsi_v4.h/.c). It seems the sensitivity of the capacitive sensors vary with the input voltage and I am thinking of using the NXP Touch Software to check if that library solves my problems.

0 Kudos
Reply
1 Solution
2,320 Views
diegovalladolid
Contributor II

After some research I see that the NXP Touch Library 2.0.0 is not compatible with KL26 despite the manual reference (NT20RM) it indeed states it is. The reason is that the library only implements the management of the TSI v5.

So here comes another question, will NXP Touch Library be compatible with KL Series in a near future?

View solution in original post

2 Replies
2,320 Views
fangli
NXP Employee
NXP Employee

Hi,

There has no any plan that Touch Library will support the KL Series. Sorry.

2,321 Views
diegovalladolid
Contributor II

After some research I see that the NXP Touch Library 2.0.0 is not compatible with KL26 despite the manual reference (NT20RM) it indeed states it is. The reason is that the library only implements the management of the TSI v5.

So here comes another question, will NXP Touch Library be compatible with KL Series in a near future?